Flash device,blank check and verify are failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flash device,blank check and verify are failed

跳至解决方案
4,223 次查看
lixinhua
Contributor I

Dear Sir ;

I'm using "MCF5272+ S29JL032J " with CodeWarrior 7.2 to develop a new product . I can't find the ARM in list of the Flash Device , and have to choice S29GL032 as substitution .I can program the MCF5272 , but we are  runuing "blank check" and "verify" are failed . Could you help us to find the root cause ? what are troubel for me to choice "flash device " ?

 

Best Regards ;

 

Tim

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,822 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tim,

If the memory you are using is not listed as part of the supported flash devices you can follow the Application Note AN3390 that explains how to add a new flash device, the document can be found on this path:

C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\Help\PDF\AddFlashDevs.pdf

Let me know if it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

在原帖中查看解决方案

0 项奖励
回复
1 回复
3,823 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tim,

If the memory you are using is not listed as part of the supported flash devices you can follow the Application Note AN3390 that explains how to add a new flash device, the document can be found on this path:

C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\Help\PDF\AddFlashDevs.pdf

Let me know if it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复