Flash device,blank check and verify are failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash device,blank check and verify are failed

ソリューションへジャンプ
4,208件の閲覧回数
lixinhua
Contributor I

Dear Sir ;

I'm using "MCF5272+ S29JL032J " with CodeWarrior 7.2 to develop a new product . I can't find the ARM in list of the Flash Device , and have to choice S29GL032 as substitution .I can program the MCF5272 , but we are  runuing "blank check" and "verify" are failed . Could you help us to find the root cause ? what are troubel for me to choice "flash device " ?

 

Best Regards ;

 

Tim

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,807件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tim,

If the memory you are using is not listed as part of the supported flash devices you can follow the Application Note AN3390 that explains how to add a new flash device, the document can be found on this path:

C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\Help\PDF\AddFlashDevs.pdf

Let me know if it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,808件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tim,

If the memory you are using is not listed as part of the supported flash devices you can follow the Application Note AN3390 that explains how to add a new flash device, the document can be found on this path:

C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\Help\PDF\AddFlashDevs.pdf

Let me know if it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信