Flash Programming fails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Programming fails

ソリューションへジャンプ
1,831件の閲覧回数
zwilcox
Contributor IV

Hello :smileyhappy:
I'm Using ColdWarrior 11 to tr to program the flash on the M54451EVB dev board.  
I'm using the USB Multilink, USB MultiLink FX, Embedded OSBDM/OSJTAG- USB connection.
I'm also using the M54451EVB_SPI.xml and M54451EVB_EXTFLASH.xml algorithm/configuration.

I get an error when I try to program the flash:

"Downloading Flash Device Driver ...
Reading flash ID .......
Error: The algorithm was not able to run on the target or the flash is not configured properly.
Error: Getting flash ID failed
Error: The algorithm was not able to run on the target or the flash is not configured properly."

flash_error.JPG

Here is a picture of my target task setup:

target_task.JPG

Here is a image of my hardware connection page:

hardware_connection.JPG

Any help would be appreciated.  Thanks :smileyhappy:

0 件の賞賛
返信
1 解決策
1,637件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Zachary,

As discussed by the internal case, you can use the linker and configuration files from a MC54451 project created in CodeWarrior 7.2 as base for your build and debug configurations.

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

元の投稿で解決策を見る

2 返答(返信)
1,637件の閲覧回数
zwilcox
Contributor IV

I've attached the configuration for the board to the post since CodeWarrior 7.2 won't run on anything passed Windows XP.  In case any one in the future runs into the problem.

carlosmendoza Thank you for your help in getting me these files.

0 件の賞賛
返信
1,638件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Zachary,

As discussed by the internal case, you can use the linker and configuration files from a MC54451 project created in CodeWarrior 7.2 as base for your build and debug configurations.

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer