Flash File to Target - Can't expand MQX_ROOT_DIR error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash File to Target - Can't expand MQX_ROOT_DIR error

ソリューションへジャンプ
3,654件の閲覧回数
video_man
Contributor III

I'm trying to flash a file (previous version compiled file) to a K70 (Tower board) from within CW 10.4. without going through the debugger.

 

I select Flash File to Target (from popup menu), it automatically provides the Flash Config File (K70FN1M0.xml), I browse to file to flash, and then select Erase and Program.

 

I receive a Target Task Error dialog box that says

 

Error executing task K70FN1M0.xml, Wrong expression ${MQX_ROOT_DIR}/lib/(etc)/init_kinetis_tcl; Could not expand variable MQX_ROOT_DIR.

 

But MQX_ROOT_DIR is already defined in Linked Resources and used for many compiler and linker search paths. And programming through Debug or Run works fine.

 

What's the problem? Is there somewhere else I need to define MQX_ROOT_DIR?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,184件の閲覧回数
video_man
Contributor III

Thanks for sending me the example project. Flash File To Target worked from your project. Having a project that worked showed the problem. I had defined a New Connection (in the Flash File To Target dialog window) and that somehow caused the MQX_ROOT_DIR error. I reset the connection to a previous connection and it works now from my project.

I don't understand why creating a New Connection caused the error. I defined it the same way as a connection that works.  But too little about CodeWarrior Eclipse makes sense to me after using CodeWarrior (classic) for 6-7 years. I suppose it's just a learning curve, but it is a painful learning curve that's killing my productivity.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,184件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hello,

does the macro is defined in the project used ?

Pascal

0 件の賞賛
返信
3,184件の閲覧回数
video_man
Contributor III

I'm not sure exactly what you are asking. The macro is defined in the project I'm using, and was defined in the project that created the compiled files. The projects compile fine and those files can be flashed using the Debug command, so the macro has to be defined correctly.

I'm trying to flash an earlier version of the code (for comparison purposes) that I saved. The Flash File to Target (from the popup menu), apparently can't use the same macro to find the init_kinetis_tcl file when executing K70FN1M0.xml. Is there another place the macro has to be defined for that process? In other words, how do you flash a file that you created previously that isn't the current version of your project?



0 件の賞賛
返信
3,183件の閲覧回数
trytohelp
NXP Employee
NXP Employee

I've a TWR-K70F120M board.

I've create a project via Project wizard for MQX for this board.

After to have rebuild the MQX lib under my MCU V10.4, I've build the project created.

I can load it via the debugger and create a Flash File to Target and it's running fine.

Extract of console:

++++++++++++++++++++++++++++++++++++++

fl::target -lc "LC for Simple Flash"

fl::target -b 0x1fff0000 0x20000

fl::target -v off -l off

cmdwin::fl::device -d "FTFE_PFlash1M0" -o "128Kx64x1" -a 0x0 0xfffff

cmdwin::fl::image -f "C:\\Temp\\Community\\307595\\MCU V10.4\\test_mqx_k70\\twrk70f120m_Int_Flash_DDRData_Debug\\test_mqx_k70.afx" -t "Auto Detect" -re on -r 0x0 0xfffff -oe off

cmdwin::fl::erase image

Beginning Operation ...   

-------------------------

Auto-detection is successful.  

  File is of type Elf Format.  

Performing target initialization ...   

Downloading Flash Device Driver ...  

Reading flash ID ...

Erasing Sector 0x00000000 to 0x00000FFF  

Erasing Sector 0x00001000 to 0x00001FFF  

Erasing Sector 0x00002000 to 0x00002FFF  

Erasing Sector 0x00003000 to 0x00003FFF  

Erasing Sector 0x00004000 to 0x00004FFF  

Erasing Sector 0x00005000 to 0x00005FFF  

Erasing Sector 0x00006000 to 0x00006FFF  

Erasing Sector 0x00007000 to 0x00007FFF  

Erasing Sector 0x00008000 to 0x00008FFF  

Erasing Sector 0x00009000 to 0x00009FFF  

Erasing Sector 0x0000A000 to 0x0000AFFF  

Erasing Sector 0x0000B000 to 0x0000BFFF  

Erasing Sector 0x0000C000 to 0x0000CFFF  

Erasing Sector 0x0000D000 to 0x0000DFFF  

Erasing ...

Erase Command Succeeded   

cmdwin::fl::write

Beginning Operation ...   

-------------------------

Using restricted address range 0x00000000 to 0x000FFFFF  

Programming file C:\Temp\Community\307595\MCU V10.4\test_mqx_k70\twrk70f120m_Int_Flash_DDRData_Debug\test_mqx_k70.afx  

Auto-detection is successful.  

  File is of type Elf Format.  

Downloading Flash Device Driver ...  

Reading flash ID ...

Auto-detection is successful.  

  File is of type Elf Format.  

Downloading 0x00000410 bytes to be programmed at 0x00000000  

Executing program ....  

Program Command Succeeded   

Downloading 0x0000D8BC bytes to be programmed at 0x00000420  

Executing program ....  

Program Command Succeeded

+++++++++++++++++++++++++++++++++

Attached you will find the project I'm using.

Regards

Pascal

3,185件の閲覧回数
video_man
Contributor III

Thanks for sending me the example project. Flash File To Target worked from your project. Having a project that worked showed the problem. I had defined a New Connection (in the Flash File To Target dialog window) and that somehow caused the MQX_ROOT_DIR error. I reset the connection to a previous connection and it works now from my project.

I don't understand why creating a New Connection caused the error. I defined it the same way as a connection that works.  But too little about CodeWarrior Eclipse makes sense to me after using CodeWarrior (classic) for 6-7 years. I suppose it's just a learning curve, but it is a painful learning curve that's killing my productivity.

0 件の賞賛
返信