Fill Memory and Global Variable Address Modifier (@address)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fill Memory and Global Variable Address Modifier (@address)

2,874件の閲覧回数
axhubner
Contributor II

Hi,

 

i am using the Global Variable Address Modifier (@address) to place eeprom variables at a specific location like:

 

const uint8 EEP_LOWER_TEMP @0x100000U = 85;

const uint8 EEP_UPPER_TEMP_MTR @0x100004U = 100;

const uint8 EEP_UPPER_TEMP_LED @0x100008U = 100;

 

We are using 4 byte aligement in the eeprom to simplify the writing. My question is how to fill the memory

between two variables? In my example i am using a 1 byte variable. The linker generates a section for each variable

witch is excatly as big as the variable. If i am using the linker to fill my whole eeprom i get conflicts with overlapping segments. If i do not fill there will be gabs in the .sx file.

 

EEPROM   = READ_ONLY   0x100000 TO 0x1007FF FILL 0xFF;

...

EEPROM_PARAM    INTO  EEPROM;

 

 

is there a solution to combine the global variable adress modifier with the fill comand?

 

Regards Axel

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,677件の閲覧回数
axhubner
Contributor II

I forgot to say that i am using a S12Z processor.

0 件の賞賛
返信

2,677件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Axel,

Could you please tell me which version of CW do you used ?

BR

Alice

0 件の賞賛
返信

2,677件の閲覧回数
axhubner
Contributor II

Hello Alice,

i am using CW 10.6.4

BR

Axel

0 件の賞賛
返信

2,677件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Axel,

What data do you want to fill between two variable ?

And i think you do not need fill it, it will be 0 ,  does 0 can not meet your demand ?

If yes, please tell me why do you want fill it .

BR

Alice

0 件の賞賛
返信