File Paths in .elf File

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

File Paths in .elf File

4,186 次查看
danielbronson
Contributor II

I am building .elf files in Codewarrior 10.6 Special Edition for Eclipse.  I am seeing file paths inside of the .elf file which are absolute paths and not relative!  This seems like a strange thing to have in a binary output of a build process!  I am even surprised that there are file paths in the file at all...

 

I am interested in having an output binary which is created exactly the same on every machine it is built on, as long as they have the same source files and IDE version.  Can I do this with the output .elf?

 

Did I miss a setting in CW IDE?  Is this common to have in output binaries?  Can someone shed a bit of experiential light on this issue? 

 

Thanks for any help in advance!

 

Dan

标签 (1)
0 项奖励
回复
3 回复数

3,533 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Daniel.

Do you want to know how to generate binary file on CW 10.6?

If not , could you show your requirement detaily ?

And which chip  ?

BR

Alice

0 项奖励
回复

3,533 次查看
danielbronson
Contributor II

Alice,

I already know how to generate the binary files on CW 10.6.  I am wondering why there are absolute paths inside of the .elf files after they are generated.  I don't have requirements: I am only curious on why the .elf file has those paths in it. 

Dan

0 项奖励
回复

3,533 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Daniel.

The .elf file is a file that can flash to the chip . In the file , there is the address and the binary data.

Could you screenshot to show what path ?

BR

Alice

0 项奖励
回复