FDRM-K82F for Master Thesis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FDRM-K82F for Master Thesis

Jump to solution
1,913 Views
armendgecaj
Contributor III

Hi all,

i have a question. Maybe someone can help me.

For my Master thesis i would like to build a vehicle that runs trough a road network and records it.

Something like Google Maps where you can see the roads.

The tasks of my vehicle should be:

  • Lane assist (so my vehicle can follow the road)
  • traffic sign recognition
  • detect pedestrian crosswalk
  • detect traffic lights
  • ......
  • .......

Is the FRDM-K82F a good choice for my master thesis?

For that board there is a demo of using the OV7670 camera. So i can save some time.

But what's about the flash memory? Mabye it's too small. Can i use an additional memory?

Thank you for your help.

Best Regards

Armend

0 Kudos
Reply
1 Solution
1,532 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Armend,

FRDM-K82F is a Freedom board with a 100LQFP K82 device. Also includes dual QuadSPI, touch pad, Arduino compatible footprint, and FlexIO header compatible with OV7670 camera.

I suggest you check this article as solution referral.

FRDM-K82F FlexIO Camera Demo 

here is an interest video.

https://community.nxp.com/docs/DOC-331060 

K82F integrated FlexBus module, it can support external flash.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,533 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Armend,

FRDM-K82F is a Freedom board with a 100LQFP K82 device. Also includes dual QuadSPI, touch pad, Arduino compatible footprint, and FlexIO header compatible with OV7670 camera.

I suggest you check this article as solution referral.

FRDM-K82F FlexIO Camera Demo 

here is an interest video.

https://community.nxp.com/docs/DOC-331060 

K82F integrated FlexBus module, it can support external flash.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply