External Memory mapping using code warrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

External Memory mapping using code warrior

跳至解决方案
2,436 次查看
narasimha
Contributor I
Hi all:smileyhappy:,
      Iam working with code warrior ,the target processor is MC68HC12A4 .I have created prm file for the existing setup. Now i would like to map the external memory using code warrior .can any one please help me out ,The existing code should be mapped to the external memory .How to create the prm file for the external memory mapping.
 
Regards
NARASIMHA
INDIA
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,751 次查看
CrasyCat
Specialist III
Hello
Look at "{Install}\(CodeWarrior_Examples)\HC12\ICD12 Target Interface\A4\AXIOM CMD12A4 Fibo - Ram - Banked"
Where {Install} stands for your installation directory.
 
This should provide you a sample prm file for a HC12A4 banked application.
 
I hope this helps
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,752 次查看
CrasyCat
Specialist III
Hello
Look at "{Install}\(CodeWarrior_Examples)\HC12\ICD12 Target Interface\A4\AXIOM CMD12A4 Fibo - Ram - Banked"
Where {Install} stands for your installation directory.
 
This should provide you a sample prm file for a HC12A4 banked application.
 
I hope this helps
 
CrasyCat
0 项奖励
回复