External Memory mapping using code warrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External Memory mapping using code warrior

ソリューションへジャンプ
2,517件の閲覧回数
narasimha
Contributor I
Hi all:smileyhappy:,
      Iam working with code warrior ,the target processor is MC68HC12A4 .I have created prm file for the existing setup. Now i would like to map the external memory using code warrior .can any one please help me out ,The existing code should be mapped to the external memory .How to create the prm file for the external memory mapping.
 
Regards
NARASIMHA
INDIA
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,832件の閲覧回数
CrasyCat
Specialist III
Hello
Look at "{Install}\(CodeWarrior_Examples)\HC12\ICD12 Target Interface\A4\AXIOM CMD12A4 Fibo - Ram - Banked"
Where {Install} stands for your installation directory.
 
This should provide you a sample prm file for a HC12A4 banked application.
 
I hope this helps
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,832件の閲覧回数
CrasyCat
Specialist III
Hello
Look at "{Install}\(CodeWarrior_Examples)\HC12\ICD12 Target Interface\A4\AXIOM CMD12A4 Fibo - Ram - Banked"
Where {Install} stands for your installation directory.
 
This should provide you a sample prm file for a HC12A4 banked application.
 
I hope this helps
 
CrasyCat
0 件の賞賛
返信