Error launching S12LZVL_FLASH_PnE U-MultiLink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error launching S12LZVL_FLASH_PnE U-MultiLink

2,630 Views
vaishakthippire
Contributor II

Hello,

I use code warrior for debugging, when I try to flash S12LZVL32 I get this below attached error. Tried to reset it but no use.  What can I do? 

Thanks!error.PNG

3 Replies

2,404 Views
RadekS
NXP Employee
NXP Employee

Hi Vaishak,

BTW: did you connect 12V power supply to your board?

The 5V from OSBDM is typically not enough for S12ZVL MCU powering.

Have a great day,
Radek

2,404 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Vaishak,

This is a general connection question. There are many possible reasons, HW and SW.

in your screenshot message box, click on "Details", what is the message?

Please also click on "Export Diagnostics" and upload here too. Thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,011 Views
cui1
Contributor II

HI Jennie Zhang

I have the same problem, Please help. Thank you

cui1_0-1706603229302.png

 

cui1_1-1706603241404.png

 

cui1_2-1706603251389.png

 

0 Kudos
Reply