Error launching S12LZVL_FLASH_PnE U-MultiLink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error launching S12LZVL_FLASH_PnE U-MultiLink

2,632件の閲覧回数
vaishakthippire
Contributor II

Hello,

I use code warrior for debugging, when I try to flash S12LZVL32 I get this below attached error. Tried to reset it but no use.  What can I do? 

Thanks!error.PNG

3 返答(返信)

2,406件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Vaishak,

BTW: did you connect 12V power supply to your board?

The 5V from OSBDM is typically not enough for S12ZVL MCU powering.

Have a great day,
Radek

2,406件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Vaishak,

This is a general connection question. There are many possible reasons, HW and SW.

in your screenshot message box, click on "Details", what is the message?

Please also click on "Export Diagnostics" and upload here too. Thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,013件の閲覧回数
cui1
Contributor II

HI Jennie Zhang

I have the same problem, Please help. Thank you

cui1_0-1706603229302.png

 

cui1_1-1706603241404.png

 

cui1_2-1706603251389.png

 

0 件の賞賛
返信