Error launching S12LZVL_FLASH_PnE U-MultiLink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error launching S12LZVL_FLASH_PnE U-MultiLink

2,695 次查看
vaishakthippire
Contributor II

Hello,

I use code warrior for debugging, when I try to flash S12LZVL32 I get this below attached error. Tried to reset it but no use.  What can I do? 

Thanks!error.PNG

3 回复数

2,469 次查看
RadekS
NXP Employee
NXP Employee

Hi Vaishak,

BTW: did you connect 12V power supply to your board?

The 5V from OSBDM is typically not enough for S12ZVL MCU powering.

Have a great day,
Radek

2,469 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Vaishak,

This is a general connection question. There are many possible reasons, HW and SW.

in your screenshot message box, click on "Details", what is the message?

Please also click on "Export Diagnostics" and upload here too. Thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,076 次查看
cui1
Contributor II

HI Jennie Zhang

I have the same problem, Please help. Thank you

cui1_0-1706603229302.png

 

cui1_1-1706603241404.png

 

cui1_2-1706603251389.png

 

0 项奖励
回复