Error importing CW10.5 file into 10.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error importing CW10.5 file into 10.6

2,128 次查看
crezyoz
Contributor IV

I am attempting to import a project done in 10.5 (K70 PE) into the latest CW 10.6

 

CW imports the file and then I get this message:

 

Invalid Workspace In Use

The current workspace has been moved or copied from a different location in the file system.

This is not supported, and can cause unpredictable behavior.  Please select another workspace.

 

 

How do I resolve that?

标签 (1)
标记 (2)
0 项奖励
回复
4 回复数

1,852 次查看
BlackNight
NXP Employee
NXP Employee

Did you move that workspace or have you copied it?

Or are you trying somehow to importe the .metadata of the workspace?

Erich

0 项奖励
回复

1,852 次查看
crezyoz
Contributor IV

The workspace was moved to a new HD after the old one died. I recreated the folder structure. (I should be able to move workspaces though. Who never has to do that? )

0 项奖励
回复

1,852 次查看
BlackNight
NXP Employee
NXP Employee

No, you *never* shall use the workspace (I mean the .metadata folder).

You can move the *projects*, but not the workspace (.metadata).

So if you do this, you will screw up things badly.

You need to create a new workspace on the new location.

You can copy/import workspace settings from the previous workspace, see Copy my workspace settings | MCU on Eclipse

The project folders inside the workspace folder you can move/copy, then import them again into your new workspace.

I hope this helps,

Erich

0 项奖励
回复

1,853 次查看
crezyoz
Contributor IV

Thanks Erich. That is so poor. I suppose I will just have to get used to it.

0 项奖励
回复