Does MC56F83000EVK support P & E?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MC56F83000EVK support P & E?

1,660 Views
d_ideologist
Contributor I

Does MC56F83000EVK support P & E? 

IF not .

I want to call the SrmCommutation function. Can I directly copy the C and H files in the PE to the src file?

Labels (1)
0 Kudos
Reply
1 Reply

1,606 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Yes, the MC56F83000-EVK supports P&E device, but it does not support USBTAP device. Pls refer to the link:

Multilink | Debug Probe | PEmicro 

You can just  connect a USB cable to the board and debug the board because there is OSJTAG device on the board based on JM60 micro-controller. But you can use the Multilink Universal device from PE to debug the board.

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply