Does MC56F83000EVK support P & E?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does MC56F83000EVK support P & E?

1,655 次查看
d_ideologist
Contributor I

Does MC56F83000EVK support P & E? 

IF not .

I want to call the SrmCommutation function. Can I directly copy the C and H files in the PE to the src file?

标签 (1)
0 项奖励
回复
1 回复

1,601 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Yes, the MC56F83000-EVK supports P&E device, but it does not support USBTAP device. Pls refer to the link:

Multilink | Debug Probe | PEmicro 

You can just  connect a USB cable to the board and debug the board because there is OSJTAG device on the board based on JM60 micro-controller. But you can use the Multilink Universal device from PE to debug the board.

Hope it can help you

BR

Xiangjun Rong

0 项奖励
回复