Disable interrupt during step CWHC08 V5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disable interrupt during step CWHC08 V5

ソリューションへジャンプ
2,475件の閲覧回数
calou
Contributor III
Hello,
 
I use CW for HC08 and the evaluation freescale card with 9s08AW60. Is it possible in the debugger to disable interrupt during step?
 
Thank you very much
 
Regards
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,573件の閲覧回数
Nabla69
Contributor V
Yes it is,
 
Simply double click on the "I" bit in the CCR Register and it will mask all maskable interrupt sources.
 
Cheers,
Alvin.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,574件の閲覧回数
Nabla69
Contributor V
Yes it is,
 
Simply double click on the "I" bit in the CCR Register and it will mask all maskable interrupt sources.
 
Cheers,
Alvin.
0 件の賞賛
返信