Device Initialization option missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device Initialization option missing

ソリューションへジャンプ
6,000件の閲覧回数
wba
Contributor III


I just updated to Codewarrior 10.4.  When I try to create a new project, I don't get the option of "Device Initialization".  I only get a selection of "None" or "Processor Expert".  Has this been removed from version 10.4 or do I not have something setup properly?

ラベル(1)
0 件の賞賛
返信
1 解決策
5,132件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Bruce,

yes, this option is not present in 10.4. You can do the same with creating a normal Processor Expert project, and then use the Init_* components.

I hope this helps.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
5,132件の閲覧回数
mylim
Contributor IV

Hi, I am using CW 10.2 installed on my Win 8 machine. I could't launch device initialization for both assembler and C project.

Te target CPU tab shows No CPU Selected with no option for me to select MCU.

I am using 10.2 because this is the last version which still supports device initialization for assembler.

Can anyone help?

Thanks.

asm project.jpgc project.jpg

0 件の賞賛
返信
5,133件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Bruce,

yes, this option is not present in 10.4. You can do the same with creating a normal Processor Expert project, and then use the Init_* components.

I hope this helps.

0 件の賞賛
返信
5,132件の閲覧回数
wba
Contributor III

Erich, thanks for the reply.

I have been using Device Initialization for years on CW6.x and CW10.x.  I guess that I will now have to do some studying and learn how to use Processor Expert Init_* components.

Some of the first differences that I have noted:

In Device Initialization, when you click on one of the modules in the "Processor" view, It brought up the component inspector for that module.  Not so in Processor Expert.

In Device Initialization, the "Processor" view had a "Generate Code".  Not so in Processor Expert.  I found "Generate Processor Expert Code" in the "Project" menu of the Hardware perspective, but, when I click on it, it says "Cannot generate - no active project selected in Project Panel.

Processor Expert projects load very slowly.

Bruce

P.S.  I enjoy your blogs on mcuoneclipse.com  It helped when I was learning to use the eclipse ide (CW10) and the Freedom board.

0 件の賞賛
返信
5,132件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Bruce,

I admit: I have not use Device Initialization much.

I do have the 'Generate Code' in the Processor view:

4662_4662.png

This is new in 10.4. So you do not have this?

If I click on a component in the Processor view, then it opens for me the inspector too:

4663_4663.png

And yes, if you use the project menu, it needs a project selected in the 'Components' view or in the 'CodeWarrior Projects view'.

Same for clicking on a component in the components view: this opens the inspector for me too.

I'm wondering why this is not the case for you?

Erich

PS: thanks :-)

0 件の賞賛
返信
5,132件の閲覧回数
wba
Contributor III

Erich,

I have found that I have to right click on the module and select "Add Component/Template".  To select a component to edit, I then click on that component in the Component view on th C/C++ perspective.  Then return to the Hardware perspective to generate code. Is that the necessary procedure?  Seems like a lot of changing perspectives and much more complicated than in Device Initialization.

Bruce


0 件の賞賛
返信
5,132件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Bruce,

I'm not using that Hardware perspective (does not make any sense to me, as I can have everything in the normal C/C++ perspective). From the C/C++ perspective you can use the menu Processor Expert > Show views to add the Processor Expert views too. And you do not have to use the Hardware perspective that way (so less perspectives, less confusion in my view). And less of problems, as I can see with your use case. The thing is that Eclipse (and Processor Expert) need to have an active project (selected). Even if you just have a single project, Eclipse needs this. If you are switching to the Hardware perspective right away, it seems that the project is not selected, so you see that problem. And the Hardware perspective does not offer a project view (where you can select the project). That makes the Hardware perspective (alone) not very useful. So I recommend that you either use the C/C++ perspective (as I do), or to add CodeWarrior Projects View (Window > Show View > ...) to your hardware perspective so you can select a project there if needed.

I hope this helps.

5,132件の閲覧回数
wba
Contributor III

Erich,

I get the same problem whether I use CW10.3 or CW10.4.

Procedure:

Start Codewarrior 10.4
create new workspace

close welcome screen

click New MCU project in Commander

enter project name

Kinetis L-series, MKL05Z8 - application

P&E Multilink

defaults

Processor Expert

Finish

Open Hardware perspective

!!!!!!!!!! Generate code & Select package now show up.  I swear they didn't before.

click on any of the modules in the Processor view and nothing happens

If I click on "Generate Processor Expert Code" in the "Project" (yes, I know that I now have it on the Processor view and that works) it says "Cannot generate - no active project selected in Project Panel

If I return to C/C++ perspective and highlight the only project then return to the Hardware perspective and do the same thing, I get the same result.

In the C/C++ perspective, If I click on any of the components in the Components view, The Components Inspector does not open.

Does yours not operate this way?

Bruce

0 件の賞賛
返信