Define a weak linkage function in Assembler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Define a weak linkage function in Assembler

2,651件の閲覧回数
-dan_l
Contributor I

I am porting an interface to the Interrupt Vector Table.    The default handler function is aliased by two weakly defined functions written in assembler, so that they may be overridden by the client code.

I cannot determine from the documentation of from the community a way to declare the function aliases as weak symbols.

If I were writing in C, this would be easy enough.

In Kinetis Design Studio a .weak directive would do the trick, but the coldfire assembler doesn't support .weak.

How does one define a symbol in ColdFire V1 assembler (using the CodeWarrior Compilation System) as a weak (aka Overload) symbol?

Thank you for your consideration!

 

0 件の賞賛
返信
1 返信

2,619件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

We have very limited resource for CF V1 assembly. All our demo code is for C. assembly is not recommended.

If you would like check assembly, you can right click on c source code, "disassemble...", you will see the generated assemble code

the assembly related documents:

1. Coldfire assembly Instruction Set:

https://www.nxp.com.cn/docs/en/reference-manual/CFPRM.pdf

2. Under CodeWarrior install folder: Assembler_CFV1_Microcontrollers.pdf

 

Have a nice day,

Jun Zhang

 

 

 

 

0 件の賞賛
返信