Debugging DPM/LSM Projects without USB NEXUS MULTILINK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging DPM/LSM Projects without USB NEXUS MULTILINK?

ソリューションへジャンプ
1,778件の閲覧回数
josephmongillo
Contributor II

I've been using an MPC5643L product for evaluation. While trying to familiarize myself with it I found a Targeting Micro-controllers pdf which included this section:

pastedImage_1.png

My question is, do I have to purchase this $400 interface in order to debug this evaluation product, or am I misunderstanding this text?

Thanks,

Joseph

1 解決策
1,688件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please write me, which board are you using with MPC5643L? If you want to program/debug the microcontroller and you have USB TRK board, you do not need any external JTAG interface.

If you use another evaluation board without USB and you want to debug/program the microcontroller, you must have external JTAG debug probe.

Please let me know.

Regards,

Martin

元の投稿で解決策を見る

2 返答(返信)
1,689件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please write me, which board are you using with MPC5643L? If you want to program/debug the microcontroller and you have USB TRK board, you do not need any external JTAG interface.

If you use another evaluation board without USB and you want to debug/program the microcontroller, you must have external JTAG debug probe.

Please let me know.

Regards,

Martin

1,688件の閲覧回数
josephmongillo
Contributor II

It is a USB TRK board, so I guess I'm good to go.

Thanks Martin!

0 件の賞賛
返信