Debugging DPM/LSM Projects without USB NEXUS MULTILINK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging DPM/LSM Projects without USB NEXUS MULTILINK?

Jump to solution
1,829 Views
josephmongillo
Contributor II

I've been using an MPC5643L product for evaluation. While trying to familiarize myself with it I found a Targeting Micro-controllers pdf which included this section:

pastedImage_1.png

My question is, do I have to purchase this $400 interface in order to debug this evaluation product, or am I misunderstanding this text?

Thanks,

Joseph

1 Solution
1,739 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please write me, which board are you using with MPC5643L? If you want to program/debug the microcontroller and you have USB TRK board, you do not need any external JTAG interface.

If you use another evaluation board without USB and you want to debug/program the microcontroller, you must have external JTAG debug probe.

Please let me know.

Regards,

Martin

View solution in original post

2 Replies
1,740 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please write me, which board are you using with MPC5643L? If you want to program/debug the microcontroller and you have USB TRK board, you do not need any external JTAG interface.

If you use another evaluation board without USB and you want to debug/program the microcontroller, you must have external JTAG debug probe.

Please let me know.

Regards,

Martin

1,739 Views
josephmongillo
Contributor II

It is a USB TRK board, so I guess I'm good to go.

Thanks Martin!

0 Kudos
Reply