Debugger cannot connect to PnE USB multilink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger cannot connect to PnE USB multilink

2,345件の閲覧回数
joonsinchu
Contributor II

Dear all,

 

I been trying to debug my code from CodeWarrior Development 10.6 through the PnE USB multilink device but it always pop out the following messages,

 

148621_148621.PNGerror1.PNG

 

148628_148628.pngerror2.png

I am currently using the chip processor of MC9RS08KB12.

My debug configurations:

 

148629_148629.jpgerror3.jpg148630_148630.jpgerror4.jpg

 

 

Hope to hear from you guys soon. I really need help urgently.

 

Thank you. appreciate your feedback .

ラベル(1)
3 返答(返信)

2,039件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Joonisn,

Does this can help you ? Problem with Multilink Rev C - not running after MCU V10.6 Update3 installed & CW for MCF V7.2

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,039件の閲覧回数
joonsinchu
Contributor II

Dear Alice,

Thanks for your info. I already updated the CW software n USB multilink version. And, i had connected all pins of the flatband cable to the BDM port of my board.

But, now there is another issue on the debugging loading time. It keep showing "Downloading 312 bytes (99%)....." without completing it. Its take up the times much more longer than the usual debugging.

Do you have any idea on this ?

cheers.

0 件の賞賛
返信

2,039件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Joonisn,

Does the board is customer board or demo board ?

And could you please test one simple project ?

Hope it helps

Alice

0 件の賞賛
返信