Debugger cannot connect to PnE USB multilink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugger cannot connect to PnE USB multilink

1,684 次查看
joonsinchu
Contributor II

Dear all,

 

I been trying to debug my code from CodeWarrior Development 10.6 through the PnE USB multilink device but it always pop out the following messages,

 

148621_148621.PNGerror1.PNG

 

148628_148628.pngerror2.png

I am currently using the chip processor of MC9RS08KB12.

My debug configurations:

 

148629_148629.jpgerror3.jpg148630_148630.jpgerror4.jpg

 

 

Hope to hear from you guys soon. I really need help urgently.

 

Thank you. appreciate your feedback .

标签 (1)
3 回复数

1,378 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Joonisn,

Does this can help you ? Problem with Multilink Rev C - not running after MCU V10.6 Update3 installed & CW for MCF V7.2

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,378 次查看
joonsinchu
Contributor II

Dear Alice,

Thanks for your info. I already updated the CW software n USB multilink version. And, i had connected all pins of the flatband cable to the BDM port of my board.

But, now there is another issue on the debugging loading time. It keep showing "Downloading 312 bytes (99%)....." without completing it. Its take up the times much more longer than the usual debugging.

Do you have any idea on this ?

cheers.

0 项奖励
回复

1,378 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Joonisn,

Does the board is customer board or demo board ?

And could you please test one simple project ?

Hope it helps

Alice

0 项奖励
回复