Debug and Mon08_Interface.ini for M68DEMOQTY

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debug and Mon08_Interface.ini for M68DEMOQTY

跳至解决方案
3,429 次查看
JM
Contributor I

In Code Warrior V5.7.0
for an assembly project created using M68HC908QT4 chip

When Debug is called, I always have to choose a device.

Is there a way to skip the <Choose Device> window ?

Also, switching from Mon08 Interface to Full Chip Simulation and back to Mon08

Interface always result in loosing connection configuration. So each time I have to

add a connection, change baud rate, change device, exit Debug, reenter Debug, choose device and connect.

Is there a way for Debug to look at the configuration file Mon08_Interface.ini and use the connection configuration and device description ?
What would be the instructions to insert in the configuration file ?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,276 次查看
FC
Contributor III

Do you have the right monitor program, there is an error supplied with the demo board.  Go to www.hc08.cz, it has good information on the 908qt4 (Nitron) mcu. 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,277 次查看
FC
Contributor III

Do you have the right monitor program, there is an error supplied with the demo board.  Go to www.hc08.cz, it has good information on the 908qt4 (Nitron) mcu. 

0 项奖励
回复