Debug and Mon08_Interface.ini for M68DEMOQTY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug and Mon08_Interface.ini for M68DEMOQTY

ソリューションへジャンプ
4,028件の閲覧回数
JM
Contributor I

In Code Warrior V5.7.0
for an assembly project created using M68HC908QT4 chip

When Debug is called, I always have to choose a device.

Is there a way to skip the <Choose Device> window ?

Also, switching from Mon08 Interface to Full Chip Simulation and back to Mon08

Interface always result in loosing connection configuration. So each time I have to

add a connection, change baud rate, change device, exit Debug, reenter Debug, choose device and connect.

Is there a way for Debug to look at the configuration file Mon08_Interface.ini and use the connection configuration and device description ?
What would be the instructions to insert in the configuration file ?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,875件の閲覧回数
FC
Contributor III

Do you have the right monitor program, there is an error supplied with the demo board.  Go to www.hc08.cz, it has good information on the 908qt4 (Nitron) mcu. 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,876件の閲覧回数
FC
Contributor III

Do you have the right monitor program, there is an error supplied with the demo board.  Go to www.hc08.cz, it has good information on the 908qt4 (Nitron) mcu. 

0 件の賞賛
返信