Debug Settings for using with Code Warrior 10.6.x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug Settings for using with Code Warrior 10.6.x

1,136 次查看
preetuabraham
Contributor III

Hi, 

 I am using the USB Multilink Universal Debugger for MC9S08AC128 with Interrupt Vectors beign used for my project.

Can I know the exact settings what needs to be configured while using debugger for Code Warrior 10.6.x. Plus The usage of Macros while usign the debugger shows errors.Like if a External interface port is used with Macro  eg:

#define PTADD _PTADD.PortData and if interrupt vectors any specific settings to be done

标签 (1)
0 项奖励
回复
1 回复

907 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Preetu,

Under the CW installation directory , there is reference manuals about use USB Multilink Universal Debugger

with CodeWarrior : CW MCU v10.6.4\MCU\Help\PDF  -> Targeting_Microcontrollers.pdf 

the part of  "Chapter 9  Connections - HCS08 Architecture -> 9.2 P&E Hardware Interface Connection for HCS08 "

Hope it helps, if still have any question , please contact me without any hesitate .


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复