Could not open memory configuration file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could not open memory configuration file

ソリューションへジャンプ
3,537件の閲覧回数
juliancox
Contributor V

I have just changed my hardware environment from DEMOQE to a USBDM connected to my S08SH target board. I have changed the debug configuration to USBDM, but when I launch DEBUG I get the message 

"Could not open memory configuration file".

When I investigate the target properties I find "The path is not valid in all configurations" and "File is invalid"

What can I do about it?

0 件の賞賛
返信
1 解決策
2,859件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Julian,

I believe it would be better if you create a new project for the S08SH MCU and develop based on this project. When you create a new project the Initialization and Memory files needed by the debugger will be added to your project inside the Debugger folder:

pastedImage_1.png

Once you have them you can use these files for your new USBDM connection following this steps:

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

pastedImage_5.png


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,859件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Julian,

Could you tell us which CodeWarrior version are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信
2,859件の閲覧回数
juliancox
Contributor V

10.7

0 件の賞賛
返信
2,860件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Julian,

I believe it would be better if you create a new project for the S08SH MCU and develop based on this project. When you create a new project the Initialization and Memory files needed by the debugger will be added to your project inside the Debugger folder:

pastedImage_1.png

Once you have them you can use these files for your new USBDM connection following this steps:

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

pastedImage_5.png


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信