Content of a .CRT file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Content of a .CRT file

1,743 次查看
FabioPdM
Contributor I

Hi, 

I have some static bytes in the source file like a stamp.

When I search for this stamp in the .crt file that will be loaded in the MC it does not exist.

Any one could help me?

0 项奖励
回复
4 回复数

1,696 次查看
FabioPdM
Contributor I

Hi Alice,

    In time, I forgot to mention that this .CRT file have 0x0D 0x0A record separators.

    Could be that this file a Freescale SRecord format?

    If so I can create it again with CW easily!!!

0 项奖励
回复

1,708 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @FabioPdM 

For better help you, please tell us the part number of your MCU, thanks.

 

 

BR

Alice

0 项奖励
回复

1,698 次查看
FabioPdM
Contributor I

Hi Alice,

      The target is MCU MC9S08AW32 and to burn it  they use a .CRT file extension that I dont know how it is created and file format.

       That's the reason that I am investigating how this file extension was created to solve the doubt.

       This file extension .CRT give any clue how can I generate it in the CW?

       The first 16 bytes in the .CRT file are ( hex 0x ) 61 69 73 64 7F 7D 43 5A 43 5D 5D 5F 44 47 5B 5E 6F 5E 73 42 ( 'aisd' )    .

       Thanks for your help!!!

0 项奖励
回复

1,670 次查看
Itzzamna_Supp
NXP TechSupport
NXP TechSupport
When compiling, S19 is generated and remains in the FLASH folder, the SRecord file type is saved there in S19, where you will find the CRT.
0 项奖励
回复