Connection error with P&E USB Multilink Universal REV B on TWRk60N512 using Codewarrior 10.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connection error with P&E USB Multilink Universal REV B on TWRk60N512 using Codewarrior 10.5

3,380 次查看
abdullahansari
Contributor III


Hallo All

 

I am trying to debug a project via USB Multilink Universal and have its connection from Port-F-Mini-20 (USB Multilink) to Cortex debug on board, with J12 settings off and power USB connected on USB MiniAB on TWR SER Board.

 

It functioned for the first time and since then its giving me following error when I am debugging it

 

9379_9379.jpgdebugerror.jpg

 

Any solution?

 

Regards

Abdullah

标签 (1)
3 回复数

2,985 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

I've performed some tests on my side.

My config is:

      Win 7 32 bit

      CodeWarrior for MCU V10.5

      P&E Multilink Universal Rev. B

      Tower Elevator + TWR-K60D100M (including a PK60DN512)

I've created 2 examples. First is using OSBDM and second Mulitlink Universal.

I'm able to load the example using OSBDM and Multink interfaces.

For Multilink Interface.

First connection

multilink_1st_debug.jpg

when  no power supply is applied on TWR-ELEV I got

multilink_debug_without_power_on_board.jpg

Now Close the debug session, switch on the power and re-launch debug.

Now it's running fine

multilink_debug_with_power_on_board.jpg

Attached the Multilink example.

Regards

Pascal

2,985 次查看
abdullahansari
Contributor III

Hi Pascal,

Thanks for the answer. I appologize for the late response. I got the problem solved as i was connecting the PE link Multilink USB wire to wrong USB Socket on the board and it wasnt powering the board up.

Regards

Abdullah

0 项奖励
回复

2,985 次查看
trytohelp
NXP Employee
NXP Employee

Hi Abdullah,

thanks for your feedback.

Regards

Pascal

0 项奖励
回复