Confusion on how to update my compiler

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Confusion on how to update my compiler

跳至解决方案
2,181 次查看
Luigi
Contributor III
I am using Codewarrior IDE, version 5.7.0, build 2015.  I need to get the header file for the 'AC16 processor.  I went to the downloads page, and it shows "Updates for CodeWarrior for HC(S)08/RS08 v5.1".  But I am running 5.7.0, so what do I download?  Thanks in advance.
 
Lou
 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,121 次查看
stanish
NXP Employee
NXP Employee
Hi Lou,

The version you refer to is just IDE version. In order to get product version you should press "Installed Products" button in the About dialog.
IDE version 5.7.0 build 2015 corresponds to  CodeWarrior v5.1. You can download AC16 Service Patch here:

http://www.freescale.com/webapp/sps/download/license.jsp?colCode=HC08-V5-1-AC16-SP&nodeId=0127260061...


Stahish

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,122 次查看
stanish
NXP Employee
NXP Employee
Hi Lou,

The version you refer to is just IDE version. In order to get product version you should press "Installed Products" button in the About dialog.
IDE version 5.7.0 build 2015 corresponds to  CodeWarrior v5.1. You can download AC16 Service Patch here:

http://www.freescale.com/webapp/sps/download/license.jsp?colCode=HC08-V5-1-AC16-SP&nodeId=0127260061...


Stahish
0 项奖励
回复
1,121 次查看
Luigi
Contributor III
Thank you!
0 项奖励
回复