Compiler syntax error for NXP files??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiler syntax error for NXP files??

3,177件の閲覧回数
pgillaspy
Contributor III

Below is the compiler errors encountered while compiling my program on CodeWarrior V11.1 with DSC QuickStart 2.7.3 for the 56F83789 processor.  The syntax error report is completely meaningless to me. This error is reported for virtually every freemaster.* source file. Please help interpret.

C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e|Compiler|Error
(C:\Users\PhilG\Hummingbird\MCE\MCESimplex\Simplex\SystemConfig\56F83789_Build_FLASH_LDM_LPM_OSJTAG.launch|1|0|1|0|1)
=<?xml version="1.0" encoding="UTF-8" standalone="no"?>
>declaration syntax error
>(included from:
> (command-line defines):1
> (C-C++ Preprocessor Panel):1
>
>C:\NXP\DSC56800EX_Quick_Start_r2.7\src\support\freemaster\freemaster_56F8xxx.c
>:1)
C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e|Compiler|Error
(C:\Users\PhilG\Hummingbird\MCE\MCESimplex\Simplex\SystemConfig\56F83789_Build_FLASH_LDM_LPM_OSJTAG.launch|1|0|1|0|1)
=<?xml version="1.0" encoding="UTF-8" standalone="no"?>
>declaration syntax error
>(included from:
> (command-line defines):1
> (C-C++ Preprocessor Panel):1
>
>C:\NXP\DSC56800EX_Quick_Start_r2.7\src\support\freemaster\freemaster_appcmd.c:
>1)
C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e|Compiler|Error
(C:\Users\PhilG\Hummingbird\MCE\MCESimplex\Simplex\SystemConfig\56F83789_Build_FLASH_LDM_LPM_OSJTAG.launch|1|0|1|0|1)
=<?xml version="1.0" encoding="UTF-8" standalone="no"?>
>declaration syntax error
>(included from:
> (command-line defines):1
> (C-C++ Preprocessor Panel):1
>
>C:\NXP\DSC56800EX_Quick_Start_r2.7\src\support\freemaster\freemaster_can.c:1)
C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e|Compiler|Error
(C:\Users\PhilG\Hummingbird\MCE\MCESimplex\Simplex\SystemConfig\56F83789_Build_FLASH_LDM_LPM_OSJTAG.launch|1|0|1|0|1)
=<?xml version="1.0" encoding="UTF-8" standalone="no"?>
>declaration syntax error
>(included from:
> (command-line defines):1
> (C-C++ Preprocessor Panel):1
>
>C:\NXP\DSC56800EX_Quick_Start_r2.7\src\support\freemaster\freemaster_fastrec.c
>:1)

0 件の賞賛
返信
4 返答(返信)

3,159件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you create a project and generate code based QuickStart tools without Freemaster device, can you compile successfully?

From your description, it appears it is a compiler option problem.

If it is convenient, pls post your project to us so that we can have a test.

BTW, we have SDK package for MC56F83xxx, which is official code generating tools.

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-s...

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信

3,155件の閲覧回数
pgillaspy
Contributor III

What do I need to do to compile without Freemaster? Delete the support/freemaster directory? Exclude support/freemaster from build?  Can you explain what Freemaster is?

0 件の賞賛
返信

3,150件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The Freemaster tools is a tools run on PC side which can display  variables in customer application via uart, Jtag, CAN or whatever interface while the application is running in LPC/Kinetis/i.mxrt... family. 

If you do not need it, you can delete all the file in Freemaster directory.

You can download Freemaster tools from the link:

https://www.nxp.com/design/software/development-software/freemaster-run-time-debugging-tool:FREEMAST...

 

Hope it can hep you

BR

XiangJun Rong

0 件の賞賛
返信

3,060件の閲覧回数
pgillaspy
Contributor III

I deleted Freemaster stuff. All is well.

0 件の賞賛
返信