Command Window 3.1 History limitation?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Command Window 3.1 History limitation?

跳至解决方案
2,958 次查看
hwrobel
NXP Employee
NXP Employee
It seems that the command history of the TCL Command Window 3.1 in CW for EPPC fills up to 250 entries and then simply stops, i.e., it neither drops the oldest entries, nor does it enlarge the history.

Does anyone know of a way to turn the history into a circular buffer, or clear it, or increase the max entry count?

Thanks!
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,338 次查看
marc_paquette
Contributor V

The command history is indeed circular. Unfortunately, the IDE doesn't adjust the command history numbers, preventing you from using the "! number" command repeat syntax in any useful way.

I've forwarded your comment along to the IDE team. I can also suggest that you submit a bug report if you'd like to keep track of this situation.

To submit a service request:

1. Go to http://freescale.com/support

2. In the Develop column, click "Technical Support."

3. Click "Submit a service request."

Marc.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,339 次查看
marc_paquette
Contributor V

The command history is indeed circular. Unfortunately, the IDE doesn't adjust the command history numbers, preventing you from using the "! number" command repeat syntax in any useful way.

I've forwarded your comment along to the IDE team. I can also suggest that you submit a bug report if you'd like to keep track of this situation.

To submit a service request:

1. Go to http://freescale.com/support

2. In the Develop column, click "Technical Support."

3. Click "Submit a service request."

Marc.

0 项奖励
回复