Command Window 3.1 History limitation?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Command Window 3.1 History limitation?

ソリューションへジャンプ
3,470件の閲覧回数
hwrobel
NXP Employee
NXP Employee
It seems that the command history of the TCL Command Window 3.1 in CW for EPPC fills up to 250 entries and then simply stops, i.e., it neither drops the oldest entries, nor does it enlarge the history.

Does anyone know of a way to turn the history into a circular buffer, or clear it, or increase the max entry count?

Thanks!
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,850件の閲覧回数
marc_paquette
Contributor V

The command history is indeed circular. Unfortunately, the IDE doesn't adjust the command history numbers, preventing you from using the "! number" command repeat syntax in any useful way.

I've forwarded your comment along to the IDE team. I can also suggest that you submit a bug report if you'd like to keep track of this situation.

To submit a service request:

1. Go to http://freescale.com/support

2. In the Develop column, click "Technical Support."

3. Click "Submit a service request."

Marc.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,851件の閲覧回数
marc_paquette
Contributor V

The command history is indeed circular. Unfortunately, the IDE doesn't adjust the command history numbers, preventing you from using the "! number" command repeat syntax in any useful way.

I've forwarded your comment along to the IDE team. I can also suggest that you submit a bug report if you'd like to keep track of this situation.

To submit a service request:

1. Go to http://freescale.com/support

2. In the Develop column, click "Technical Support."

3. Click "Submit a service request."

Marc.

0 件の賞賛
返信