Command Line on-board flash programmer for 9S12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Command Line on-board flash programmer for 9S12

跳至解决方案
3,708 次查看
darrin
Contributor II
Hello,
 
I am using CodeWarrior 4.5 for the 9S12 and the P&E USB multilink programmer.
I can program the on-board flash by clicking "debug" in the IDE which calls hiwave debugger.
Is there a command-line way to program the on-board 9S12 flash?
 
Thanks
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,818 次查看
CrasyCat
Specialist III
Hello
 
We do not have command line tools to do production flash programming.
If you are looking for production flash programming tool you can check with P&E (www.pemicro.com).
 
They have production flash programming tools for HCS12.
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,819 次查看
CrasyCat
Specialist III
Hello
 
We do not have command line tools to do production flash programming.
If you are looking for production flash programming tool you can check with P&E (www.pemicro.com).
 
They have production flash programming tools for HCS12.
 
CrasyCat
0 项奖励
回复