Command Line on-board flash programmer for 9S12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Command Line on-board flash programmer for 9S12

Jump to solution
3,717 Views
darrin
Contributor II
Hello,
 
I am using CodeWarrior 4.5 for the 9S12 and the P&E USB multilink programmer.
I can program the on-board flash by clicking "debug" in the IDE which calls hiwave debugger.
Is there a command-line way to program the on-board 9S12 flash?
 
Thanks
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,827 Views
CrasyCat
Specialist III
Hello
 
We do not have command line tools to do production flash programming.
If you are looking for production flash programming tool you can check with P&E (www.pemicro.com).
 
They have production flash programming tools for HCS12.
 
CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
1,828 Views
CrasyCat
Specialist III
Hello
 
We do not have command line tools to do production flash programming.
If you are looking for production flash programming tool you can check with P&E (www.pemicro.com).
 
They have production flash programming tools for HCS12.
 
CrasyCat
0 Kudos
Reply