Codewarrior without Eclipse?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior without Eclipse?

1,683件の閲覧回数
Lundin
Senior Contributor IV

I would like to know if there are any plans to develop Eclipse-free versions of Codewarrior for HS08 in the near future. I don't want Eclipse, and since I have recently gotten fed a Windows 7/64 PC, I now have to run classic CW in some icky Windows XP emulator.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,479件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The simple answer is: there are no such plans.

But you are free to use any IDE as the compiler/build tools are command line based.

0 件の賞賛
返信

1,479件の閲覧回数
Lundin
Senior Contributor IV

But the 5.9.0 version of the IDE already supports Windows 7/64. It can't be that much work to update the S08 compiler for this IDE as well. Eclipse is not an option. If there are no plans of upgrading, I suppose I'll have to either get a 3rd party compiler or specify a different MCU brand.

0 件の賞賛
返信