Codewarrior without Eclipse?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior without Eclipse?

1,689 Views
Lundin
Senior Contributor IV

I would like to know if there are any plans to develop Eclipse-free versions of Codewarrior for HS08 in the near future. I don't want Eclipse, and since I have recently gotten fed a Windows 7/64 PC, I now have to run classic CW in some icky Windows XP emulator.

Labels (1)
0 Kudos
Reply
2 Replies

1,485 Views
BlackNight
NXP Employee
NXP Employee

The simple answer is: there are no such plans.

But you are free to use any IDE as the compiler/build tools are command line based.

0 Kudos
Reply

1,485 Views
Lundin
Senior Contributor IV

But the 5.9.0 version of the IDE already supports Windows 7/64. It can't be that much work to update the S08 compiler for this IDE as well. Eclipse is not an option. If there are no plans of upgrading, I suppose I'll have to either get a 3rd party compiler or specify a different MCU brand.

0 Kudos
Reply