Codewarrior under VMware randomly thinks it unlicensed (when licensed by disk ID)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Codewarrior under VMware randomly thinks it unlicensed (when licensed by disk ID)

跳至解决方案
2,491 次查看
TrevK
Contributor I
Hi,

I'm running the "Codewarrior for HC12 V4.6" command line compiler under VMware server 1.05 in a guest XP SP2 box for our nightly builds.

This has been working fine for months but occassionally Codewarrior thinks it is no longer licensed ("ERROR C5300: Limitation: code size 4577 > 1024 bytes").

This machine is licensed based on disk ID (rather than Ethernet MAC), and obviously the C: disk volume ID hasn't changed.

Has anyone else seen this sort of problem?

Sometimes a reboot will cure this (Our guest XP virtual machine is also configured to reboot everyday at 1:30am), but sometimes not. We have not managed to track down why this is failing.

Note, we've seen the same issue when hosting under VMware server on Linux, and VMware server on Windows.

Any ideas much appreciated.
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,485 次查看
J2MEJediMaster
Specialist I
I'd speculate that perhaps VMware might not deliver a request for reading the disk ID in a timely manner might be at fault here. But that's just speculation, which isn't helping you. I'd suggest that you submit a SR on the problem by clicking here.

---Tom

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,486 次查看
J2MEJediMaster
Specialist I
I'd speculate that perhaps VMware might not deliver a request for reading the disk ID in a timely manner might be at fault here. But that's just speculation, which isn't helping you. I'd suggest that you submit a SR on the problem by clicking here.

---Tom
0 项奖励
回复