Codewarrior under VMware randomly thinks it unlicensed (when licensed by disk ID)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior under VMware randomly thinks it unlicensed (when licensed by disk ID)

Jump to solution
2,487 Views
TrevK
Contributor I
Hi,

I'm running the "Codewarrior for HC12 V4.6" command line compiler under VMware server 1.05 in a guest XP SP2 box for our nightly builds.

This has been working fine for months but occassionally Codewarrior thinks it is no longer licensed ("ERROR C5300: Limitation: code size 4577 > 1024 bytes").

This machine is licensed based on disk ID (rather than Ethernet MAC), and obviously the C: disk volume ID hasn't changed.

Has anyone else seen this sort of problem?

Sometimes a reboot will cure this (Our guest XP virtual machine is also configured to reboot everyday at 1:30am), but sometimes not. We have not managed to track down why this is failing.

Note, we've seen the same issue when hosting under VMware server on Linux, and VMware server on Windows.

Any ideas much appreciated.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,481 Views
J2MEJediMaster
Specialist I
I'd speculate that perhaps VMware might not deliver a request for reading the disk ID in a timely manner might be at fault here. But that's just speculation, which isn't helping you. I'd suggest that you submit a SR on the problem by clicking here.

---Tom

View solution in original post

0 Kudos
Reply
1 Reply
1,482 Views
J2MEJediMaster
Specialist I
I'd speculate that perhaps VMware might not deliver a request for reading the disk ID in a timely manner might be at fault here. But that's just speculation, which isn't helping you. I'd suggest that you submit a SR on the problem by clicking here.

---Tom
0 Kudos
Reply