Codewarrior - DSC comparator example for 56F84789

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior - DSC comparator example for 56F84789

Jump to solution
1,951 Views
TurboMan
Contributor IV

Hi,

  does anyone have a comparator example using codewarrior for the 56F84789? Cannot find a CodeWarrior example that works for me.

 

Secondly, what's with Freescale communities these days? Where's the DSC category? This is the closest I can get. It's making help/support very hard to find, so apologies if this is in the wrong section...

Labels (1)
0 Kudos
Reply
1 Solution
1,689 Views
TICS_Fiona
NXP Employee
NXP Employee

Hi

I attached an example project for 56F8257 which has the same comparator with 56F84789, you can use it as a reference.

The link for DSC in community is:

https://community.freescale.com/community/dsc/content

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,690 Views
TICS_Fiona
NXP Employee
NXP Employee

Hi

I attached an example project for 56F8257 which has the same comparator with 56F84789, you can use it as a reference.

The link for DSC in community is:

https://community.freescale.com/community/dsc/content

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply