Codewarrior - DSC comparator example for 56F84789

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior - DSC comparator example for 56F84789

ソリューションへジャンプ
1,318件の閲覧回数
TurboMan
Contributor IV

Hi,

  does anyone have a comparator example using codewarrior for the 56F84789? Cannot find a CodeWarrior example that works for me.

 

Secondly, what's with Freescale communities these days? Where's the DSC category? This is the closest I can get. It's making help/support very hard to find, so apologies if this is in the wrong section...

ラベル(1)
0 件の賞賛
返信
1 解決策
1,056件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hi

I attached an example project for 56F8257 which has the same comparator with 56F84789, you can use it as a reference.

The link for DSC in community is:

https://community.freescale.com/community/dsc/content

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,057件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hi

I attached an example project for 56F8257 which has the same comparator with 56F84789, you can use it as a reference.

The link for DSC in community is:

https://community.freescale.com/community/dsc/content

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信