CodeWarriorHC(S)08 3.1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarriorHC(S)08 3.1?

4,788 Views
JimT
Contributor I
Is CodeWarriror HC(S)08 V3.1 Special Edition still available for download?  I am unable to find it.  I've recently joined a project where all of the developers are using that version and I would like to as well.


Labels (1)
Tags (1)
0 Kudos
Reply
6 Replies

2,763 Views
Alban
Senior Contributor II
Hello,

Special Edition is the Free one.
Therefore I don't see any special reason to keep using the CW08 3.1.

If you explain why you cannot upgrade to the also free but richer featured CWMCU 6.0, I may be able to find a download for you.

Cheers,
Alban.

0 Kudos
Reply

2,763 Views
JimT
Contributor I
Since other members of the project are using 3.1, I wanted to as well so that I could share project files back and forth with them.  Since I am the newcomer to their development I didn't want to be a disruption, and it appeared they could not load "project" files that I created with a newer version.


0 Kudos
Reply

2,763 Views
Alban
Senior Contributor II
Ok,

I'll see what I can do to temporarily make it available.
Do you have a high speed internet connection to download 161MB ?

Alban.
0 Kudos
Reply

2,763 Views
Alban
Senior Contributor II
Hello,

I put the file available on my personal server especially for you. It should be uploaded at 11pm GMT+1.
As you did not put the targeted MCU (a basic required info) I could not put any patch. They should be available from CodeWarrior website or via the updater.
Please note that the file will be deleted in a couple of days.
http://fsl.k-noo.net/CW08_31/

Do notify me when your download is complete.

Hope this helps,
Alban.
0 Kudos
Reply

2,763 Views
JimT
Contributor I
Great.  Got it.  Thank you for your help.

0 Kudos
Reply

2,763 Views
Nouchi
Senior Contributor II
Hi,

CW 3.1 is no longer available, but you can download CW for MCU V6.0 Special edition (support for HC(S)08 family and coldfire V1).
http://www.freescale.com/webapp/Download?colCode=CWX-HC08-SE&nodeId=01272600610BF1&location=overview



Emmanuel
0 Kudos
Reply