CodeWarrior installation problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior installation problems

ソリューションへジャンプ
2,236件の閲覧回数
ycgxy1650601
Contributor III

hi:

I want to use CodeWarrior IDE(v2.10) for MCP5606B.

Today,I download the trial software(CodeWarrior for MPC55xx/MPC56xx - Professional Edition Evaluation / Updates ).And I have finished the installation.

Now,I have two questions:

   first,I Install CodeWarrior IDE(v2.10) one by one,According to the  above link.Is it right?

   second,Is the information of the below picture right,when I finish the installtion?

CW210IDE About内容.JPG

third,Can I install two different versions about CodeWarrior,on same computer ?(for example:v2.10 and v5.1)

thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,187件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

first,I Install CodeWarrior IDE(v2.10) one by one,According to the  above link.Is it right?

- yes, correct.

second,Is the information of the below picture right,when I finish the installtion?

- yes, correct.

third,Can I install two different versions about CodeWarrior,on same computer ?(for example:v2.10 and v5.1)

- yes, you can have more versions of CodeWarrior installed on the same computer.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,188件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

first,I Install CodeWarrior IDE(v2.10) one by one,According to the  above link.Is it right?

- yes, correct.

second,Is the information of the below picture right,when I finish the installtion?

- yes, correct.

third,Can I install two different versions about CodeWarrior,on same computer ?(for example:v2.10 and v5.1)

- yes, you can have more versions of CodeWarrior installed on the same computer.

Regards,

Lukas

0 件の賞賛
返信