CodeWarrior for HCS12 logical and physical addresses

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for HCS12 logical and physical addresses

Jump to solution
2,238 Views
shadoooo
Contributor I
Hi.
I need to develop a bootloader for HCS12 microcontrollers (9S12A256 and 9SA64).
I need some information about the addresses used in the S19 files generated by the linker, in both logical and physical addressing mode.
We have in production PEMICRO prog12z, and we are using log2phy to convert the addresses from logical to physical. However, I don't understand very well the convertion operations: where do I find the page address convertion tables between logical and physical?
Is log2phy target file identical to the one generated by CW?
Thanks
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,118 Views
J2MEJediMaster
Specialist I
0 Kudos
Reply
1 Reply
1,119 Views
J2MEJediMaster
Specialist I
Check out the information on this forum: http://www.embeddedrelated.com/groups/68hc12/show/3014.php

---Tom

0 Kudos
Reply