CodeWarrior for HCS12 logical and physical addresses

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for HCS12 logical and physical addresses

ソリューションへジャンプ
3,006件の閲覧回数
shadoooo
Contributor I
Hi.
I need to develop a bootloader for HCS12 microcontrollers (9S12A256 and 9SA64).
I need some information about the addresses used in the S19 files generated by the linker, in both logical and physical addressing mode.
We have in production PEMICRO prog12z, and we are using log2phy to convert the addresses from logical to physical. However, I don't understand very well the convertion operations: where do I find the page address convertion tables between logical and physical?
Is log2phy target file identical to the one generated by CW?
Thanks
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,886件の閲覧回数
J2MEJediMaster
Specialist I
0 件の賞賛
返信
1 返信
1,887件の閲覧回数
J2MEJediMaster
Specialist I
Check out the information on this forum: http://www.embeddedrelated.com/groups/68hc12/show/3014.php

---Tom

0 件の賞賛
返信