CodeWarrior V3.0 with Cyclone Pro?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior V3.0 with Cyclone Pro?

跳至解决方案
2,260 次查看
ThomasH
Contributor II
 
I have to program/debug a HC08 system. For this I have the CodeWarrior V3.0 and a P&E Cyclone Pro. If I want to debug the HC08 I´m not able to select the Cyclone Pro (connected with USB to the PC) There is only the possibility to select a COM port. But If I use a COM port the Cyclone Pro crashes (display and led´s dark, buttons no reaction).
So is it possible that the CodeWarrior V3.0 for HC08 does not support the actual CyclonePro?
 
Thanks and best regards
Thomas
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,275 次查看
J2MEJediMaster
Specialist I
I think for USB support you'll need CodeWarrior 3.1.

---Tom

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,276 次查看
J2MEJediMaster
Specialist I
I think for USB support you'll need CodeWarrior 3.1.

---Tom
0 项奖励
回复
1,275 次查看
ThomasH
Contributor II
I have also tried it with the serial port (Class V - P&E Cyclone interface...) but there the error message "P&E MON08 interface not detected...." appears. In this case the Cyclone´s display and LED´s are completely dark till I close the COM port.
0 项奖励
回复