CodeWarrior V3.0 with Cyclone Pro?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior V3.0 with Cyclone Pro?

ソリューションへジャンプ
3,082件の閲覧回数
ThomasH
Contributor II
 
I have to program/debug a HC08 system. For this I have the CodeWarrior V3.0 and a P&E Cyclone Pro. If I want to debug the HC08 I´m not able to select the Cyclone Pro (connected with USB to the PC) There is only the possibility to select a COM port. But If I use a COM port the Cyclone Pro crashes (display and led´s dark, buttons no reaction).
So is it possible that the CodeWarrior V3.0 for HC08 does not support the actual CyclonePro?
 
Thanks and best regards
Thomas
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,097件の閲覧回数
J2MEJediMaster
Specialist I
I think for USB support you'll need CodeWarrior 3.1.

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,098件の閲覧回数
J2MEJediMaster
Specialist I
I think for USB support you'll need CodeWarrior 3.1.

---Tom
0 件の賞賛
返信
2,097件の閲覧回数
ThomasH
Contributor II
I have also tried it with the serial port (Class V - P&E Cyclone interface...) but there the error message "P&E MON08 interface not detected...." appears. In this case the Cyclone´s display and LED´s are completely dark till I close the COM port.
0 件の賞賛
返信