CodeWarrior V3.0 with Cyclone Pro?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior V3.0 with Cyclone Pro?

Jump to solution
3,056 Views
ThomasH
Contributor II
 
I have to program/debug a HC08 system. For this I have the CodeWarrior V3.0 and a P&E Cyclone Pro. If I want to debug the HC08 I´m not able to select the Cyclone Pro (connected with USB to the PC) There is only the possibility to select a COM port. But If I use a COM port the Cyclone Pro crashes (display and led´s dark, buttons no reaction).
So is it possible that the CodeWarrior V3.0 for HC08 does not support the actual CyclonePro?
 
Thanks and best regards
Thomas
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,071 Views
J2MEJediMaster
Specialist I
I think for USB support you'll need CodeWarrior 3.1.

---Tom

View solution in original post

0 Kudos
Reply
2 Replies
2,072 Views
J2MEJediMaster
Specialist I
I think for USB support you'll need CodeWarrior 3.1.

---Tom
0 Kudos
Reply
2,071 Views
ThomasH
Contributor II
I have also tried it with the serial port (Class V - P&E Cyclone interface...) but there the error message "P&E MON08 interface not detected...." appears. In this case the Cyclone´s display and LED´s are completely dark till I close the COM port.
0 Kudos
Reply