12-27-2007
08:15 PM
2,473 次查看

What_lezhich
Contributor I
Hello People,
I have installed the CodeWarrior without any problems.
When I turn on the program I get a startup window in which I choose the "Create Project" button, afterwards, I choose the MCU I use, at the next window I choose the language and the project's destination, when I push the "Next" button, the system crushes and "kicks" me out by turning itself off.
Also, by pushing the "Run Getting Started Tutorial" button at the startup window, I am getting the same results...
I tried to install the software at other computer and there were no problems.
Does anybody know what may be the reason for such effect and how do I solve this task?
Thank you in advance.
已解决! 转到解答。
1 解答
12-28-2007
07:45 PM
1,022 次查看


NXP Employee
The search is at the bottom of this webpage :smileyhappy:
When searching for Groove, here's a direct link with the Groove bug workaround:
http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...
Given your description I don't have the impression it is the Groove incompatibility though.
Which os are you using, you did not mention it AFAIS.
And CW for MCU's 6.1 can be downloaded from www.freescale.com, download the "Special Edition".
Daniel
When searching for Groove, here's a direct link with the Groove bug workaround:
http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...
Given your description I don't have the impression it is the Groove incompatibility though.
Which os are you using, you did not mention it AFAIS.
And CW for MCU's 6.1 can be downloaded from www.freescale.com, download the "Special Edition".
Daniel
4 回复数
12-27-2007
09:39 PM
1,022 次查看


NXP Employee
Which OS are you using?
There are compatibility issues with Microsoft's Groove, part of Microsoft's office tools. Do you have them installed, if so seach this forum for the workaround.
Also does the current CW for MCU's 6.1 behave better, did you try that current version?
Did you get any dump files?
Daniel
There are compatibility issues with Microsoft's Groove, part of Microsoft's office tools. Do you have them installed, if so seach this forum for the workaround.
Also does the current CW for MCU's 6.1 behave better, did you try that current version?
Did you get any dump files?
Daniel
12-28-2007
09:42 AM
1,022 次查看

What_lezhich
Contributor I
Hi,
I'm sorry but I have no idea about where should I check for those installed "compatibility issues with Microsoft's Groove". I would be greatful if you could guide me where to search.
About the 6.1 version, I dont have it. All I have is the version I got from my university (v5.1). Also, would you tell me where I can get one (IF I can get one)?
Thanks alot,
Oleg.
12-28-2007
07:45 PM
1,023 次查看


NXP Employee
The search is at the bottom of this webpage :smileyhappy:
When searching for Groove, here's a direct link with the Groove bug workaround:
http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...
Given your description I don't have the impression it is the Groove incompatibility though.
Which os are you using, you did not mention it AFAIS.
And CW for MCU's 6.1 can be downloaded from www.freescale.com, download the "Special Edition".
Daniel
When searching for Groove, here's a direct link with the Groove bug workaround:
http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...
Given your description I don't have the impression it is the Groove incompatibility though.
Which os are you using, you did not mention it AFAIS.
And CW for MCU's 6.1 can be downloaded from www.freescale.com, download the "Special Edition".
Daniel
12-29-2007
10:33 AM
1,022 次查看

What_lezhich
Contributor I
Allrighty....!!!!! 

All I had to do is to uncheck the "Run this program in compatibility mode for" in the compatibility tab of IDE.exe properties (like it was said in the link you gave me). From now and on, the program works like a Swiss watch 

Thank you very much for your help, Daniel.