CodeWarrior Development Studio for ColdFire Architectures, Linux Edition, Version 2.3.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior Development Studio for ColdFire Architectures, Linux Edition, Version 2.3.

跳至解决方案
3,821 次查看
WimC
Contributor I
Hello all,

is the CodeWarrior linux edition working with the Coldfire 5213? I want to make a new project for the 5213 but i cant find the coldfire templates.

Thanx for the help.

Greets, Wim
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,539 次查看
CrasyCat
Specialist III
Hello
 
As far as CodeWarrior Linux edition is concerned, there are two editions available.
  - Application Edition. This one allows you to develop applications running on top of an embedded Linux.
  - Platform edition: This one allows you to debug the kernel itself and also includes features from the
     Application edition.
 
Basic Requirement is that you have an embedded Linux kernel running on your target board.
Note that they do not work with ucLinux kernel.
 
What kind of BSP do you have running on your board?
 
If you go to the CodeWarrior For ColdFire Linux Edition web page, you find the
"CodeWarrior Development Studio for ColdFire Architectures, Linux Edition Targeting Manual".
This manual should also be part of your installation layout.
 
In Chapter "Introduction" there is a section "Supported Target Boards" describing which boards are supported by the version.
 
I hope this helps.
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,539 次查看
CrasyCat
Specialist III
Hello
 
Which CodeWarrior Linux Product did you install?
Are you using
"CodeWarrior™ Development Studio for Power Architecture™ Processors, Linux Application Edition"
"CodeWarrior™ Development Studio for Power Architecture™ Processors, Linux Platform Edition"
 
These products are for MPC targets only.
 
CrasyCat
0 项奖励
回复
2,539 次查看
WimC
Contributor I
working with:

CodeWarrior Development Studio for ColdFire Architectures, Linux Edition, Version 2.3.
0 项奖励
回复
2,540 次查看
CrasyCat
Specialist III
Hello
 
As far as CodeWarrior Linux edition is concerned, there are two editions available.
  - Application Edition. This one allows you to develop applications running on top of an embedded Linux.
  - Platform edition: This one allows you to debug the kernel itself and also includes features from the
     Application edition.
 
Basic Requirement is that you have an embedded Linux kernel running on your target board.
Note that they do not work with ucLinux kernel.
 
What kind of BSP do you have running on your board?
 
If you go to the CodeWarrior For ColdFire Linux Edition web page, you find the
"CodeWarrior Development Studio for ColdFire Architectures, Linux Edition Targeting Manual".
This manual should also be part of your installation layout.
 
In Chapter "Introduction" there is a section "Supported Target Boards" describing which boards are supported by the version.
 
I hope this helps.
 
CrasyCat
0 项奖励
回复
2,539 次查看
WimC
Contributor I
I found it. The 5213 is not supported. Thanx for the help.

Greets, Wim
0 项奖励
回复