Code Warrior Debugger Busy Adding variables to Data1 Window

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior Debugger Busy Adding variables to Data1 Window

ソリューションへジャンプ
2,765件の閲覧回数
anil
Contributor I
Subject: Description: When starting the debugger, the command file is busy repeating the commands over and over for 15 minutes or so. Data:1 ADDXPR "batt[1]" !Data:1 ADDXPR "batt[0].fault_u.u16" !Data:1 ADDXPR "fault_system_u.u16" !Data:1 ADDXPR "fault_port_u[0].u8" !Data:1 ADDXPR "av_rx_pkt_u[0].data[1]" This problem seemed to occur after I installed 4.5 on my system. 3.1 now is doing this also. This is making it real difficult to debug. I have NOT changed any of the .cmd files to cause this problem.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,956件の閲覧回数
CrasyCat
Specialist III
Hello
 
Can you try the following.
Close the debugger.
In the directory where the .abs file is generated (usually {Project}\bin) you have a file with extension .xpr.
Delete it and try debugging again.
 
Does it help?
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,956件の閲覧回数
anil
Contributor I
Thanks...that worked.
0 件の賞賛
返信
1,957件の閲覧回数
CrasyCat
Specialist III
Hello
 
Can you try the following.
Close the debugger.
In the directory where the .abs file is generated (usually {Project}\bin) you have a file with extension .xpr.
Delete it and try debugging again.
 
Does it help?
 
CrasyCat
0 件の賞賛
返信